THE DECENTRALIZED INSTALLATION PHILOSOPHY

A pluggable, decentralized installation is clearly structured, requires fewer resources, and remains flexible throughout the service life of the building.

SHORTAGE OF SKILLED WORKERS DRIVES BUILDING INDUSTRY INTO CRISIS - 
PLUGGABLE ELECTRICAL INSTALLATION OFFERS THE SOLUTION 

A meaningful indicator of an increasing shortage of skilled workers is the development of general employment figures in the German economy, particularly in the electrical sector.

But an ostrich policy in view of the current situation would be fatal. Instead of resignation, rethinking will help – especially among those responsible in the planning offices, since they act in their function as a link between building owners, investors, architects and users. They will put conventional electrical installation methods to the test from a cost-benefit perspective. 

And they will ask themselves: 

How can new building concepts on the one hand and changes in existing utilization concepts on the other be realized faster, more flexibly and more simply than in the past when time, personnel and financial resources are tight?

THE ANSWER:  
DECENTRALIZED AND PLUGGABLE ELECTRICAL INSTALLATION SYSTEMS

Unfortunately, the majority of today's electrical installations are still made in the conventional way, and thus in a star configuration. But what is the problem here? A metaphor.

A LOOK AT NATURE

If a tree in nature were to act according to the same principle, the result would look something like this:

THE CRUX OF THE MATTER:

All leaves need to be supplied by the soil individually.

THE CONSEQUENCE:

Little efficiency with 
high space requirements 
and material usage.

BUT WHAT IF...

the energy distribution does not have to supply all consumers individually, as in nature, but instead supplies all leaves via a single trunk.

THE HAPPY RESULT:

  • Less material used
  • Higher energy efficiency
  • Less space required
  • Reduced fire load

 CONVENTIONAL VS. DECENTRALIZED ELECTRICAL INSTALLATION

CONVENTIONAL 
INSTALLATION

Conventional features: 

  • Star-shaped arrangement of the installation
  • Each consumer is connected to the subdistribution through a line
  • Electrician must connect everything himself on site
  • High material input
  • High space requirement in the installation zones and the subdistribution board

The moment maintenance or changes to the existing utilisation concept are due, at the latest, it becomes clear: nerve-racking work steps are inevitable, time-consuming and cost-intensive installation processes are imminent and tie up not only financial resources but also valuable personnel capacities.

DECENTRALIZED ELECTRICAL INSTALLATION

Decentralized features: 

  • Supply takes place via a central line with a higher cross-section
  • Individual consumers are supplied via distributors
  • From the subdistribution, a stepwise (fused) cross-sectional distribution is provided

THIS MEANS:

Reduction of the line length by up to 80%

Copper savings of up to 66%

A complex power supply or room automation can only be simplified if a decentralized cabling structure is implemented. In combination with the pluggability, this results in a system that can be installed quickly and safely. In concrete terms, this means that the complexity of the cabling is greatly reduced, which increases the clarity of the installation and greatly simplifies changes or extensions. As a result, individual components can be installed separately from one another, expanded into a clearly structured system in just a few steps, and thus also better maintained.

TO THE POINT:

With careful planning, decentralization simplifies the project process so that the effort is balanced out by reduced times for execution, project monitoring and troubleshooting.

ENERGY AND COST SAVINGS 

...during the construction and life cycle of a building, thanks to three-phase cabling right up to the consumers:

  1. A structured and clear cabling is created
  2. Reduction of the copper content due to lower line costs
  3. Increase in flexibility for extensions and changes
  4. Increase in net floor area, thanks to smaller subdivisions.
  5. Reduction of voltage drop and fire load

EVERYTHING FROM A SINGLE SOURCE:

With our installation connector system gesis® & RST® we offer all components for a decentralized and pluggable electrical installation in a modular system from one source.

Backbone: gesis® NRG

 
Decentralized installation room: gesis® RAN distribution box
 


gesis® & RST® installation connectors:  Interfaces to the field level 

APPLICATION AREAS  
OF DECENTRALIZED ELECTRICAL INSTALLATION 

1. OFFICE BUILDING

Initial situation: Conventional office areas are characterized by a rather rigid office layout, which turns out to be not very adaptable – especially to unforeseen events.

Modern office spaces are designed to allow for flexible space concepts and must be effectively convertible, especially with regard to:

  • Number of employees (reduction or increase of work stations)
  • Functionality (e.g. open-plan offices, separation of discrete spaces in the form of individual offices, meeting, conference or brainstorming rooms)
  • Room automation (lighting, air conditioning, sun protection)

To implement a well thought-out and future-proof office architecture, the decentralized & pluggable electrical installation is the ideal solution:

The entire energy supply, along with lighting installation, climate control and room automation, can be networked via a decentralized, smart electrical installation: the pluggable concept ensures clear structures, because cabling and plug-in systems are quickly installed and easy to handle. The necessary installation space for controllers, protection/switching devices, etc. is provided by the Wieland distribution boxes, which are installed in the suspended ceiling or in the false floor and connected in a plug-in manner. The advantages are clear: No more headaches about how future office concepts can actually be implemented. The business benefits are obvious, not only for the office operator, but above all for planners and installers, namely reduced time and costs with increased effectiveness.

2. SHOPFITTING

Anyone who wants to plan and operate a modern and efficient store system cannot avoid a clear structure through modular installation. It offers more security, because not only is maintenance or even repair made easier, but also subsequent adjustments and extensions can be implemented quickly. The prerequisite here is that all components are designed to be pluggable. 

Advantages – for both planners and installers – of decentralized & pluggable infrastructure cabling in shopfitting are:

  • Decentralized energy supply
  • Energy taps at any position on the sales floor
  • No manually wired junction boxes

 

Specific potential for optimization lies primarily in the areas of:

  • Shelving systems
  • Lighting
  • Infrastructure cabling

3. FUNCTIONAL BUILDINGS

Nowadays, a wide variety of usage structures are required in almost all functional buildings.

This is especially true for the following types of buildings:

  • Office and administration building
  • Education: Kindergartens, schools, universities
  • Healthcare: Hospitals, nursing homes

 

Your advantages for functional buildings:

  • Shorter planning and realization times
  • Reduction of the complexity of the entire electrical installation
  • Clear structures in energy supply
  • Holistic sustainability
  • More flexibility for changes of use

In general, functional buildings present planning offices and installers with a very special challenge when it comes to electrical installation, because the following obstacles make planning and implementation more difficult:

  • Lack of clarity: The complex requirements make a structured implementation of the installation necessary
  • Interconnectedness: Although most functional buildings are divided into individual areas, they must be strongly interconnected. Everything is connected to everything else, but must also function separately
  • Momentum: In the life cycle, functional buildings undergo minor or major changes of use. These changes are not always predictable in the long term, making rapid responses necessary
  • Lack of transparency: In the case of functional buildings, not all information about the different building or usage areas is always accessible
  • Multi-purpose: Purpose-built buildings are generally "multi-purpose buildings", i.e. they have a variety of different spatial concepts, each of which must first fulfill its own specific task and must also be integrated into the overall concept

The answer to these challenges:

Pluggable and decentralized electrical installation systems!

HAVE WE AROUSED YOUR INTEREST?

Download our free concept paper with all the information!  

Pluggable installation systems – save time and become more flexible!


DOWNLOAD now for free

Whitepaper "Steckbare Installationssysteme"

YOU HAVE QUESTIONS?
WE CAN ANSWER!

"Wieland distribution boxes support an intelligent building right down to the installation level. They ensure easy decentralized handling of the automation systems needed to increase energy efficiency and help ensure that the electrical installation also earns the title of Smart Building Ready."

TOBIAS HENNEMANN 
BUILDING SOLUTIONS PRODUCT MANAGER 

Tobias Hennemann
contact

Do you need further product information?

Please contact our experts.

call: +49 951 9324 996

send request
callback service